Download
Search for Software for Controllers Motion Controllers
Setting/programming products - Motion control setting - Motion control setting
Motion control setting (English)
Back to the list screen
Notifications
- When using version 1.005F or later, data cannot be written to a Motion module which has a motion system software version of 04 or earlier.
When using version 1.005F or later, update the motion system software to version 05 or later.
to download MELSEC iQ-R Motion module motion system software.
- Data that was saved using version 1.005F or later cannot be edited and browsed in an environment where version 1.001B or earlier of the motion control setting is installed.
- To use version 1.040S or later, GX Works3 version 1.085P or later must be installed.
- Version 1.040S or later does not support CW Configurator Version1. When using CW Configurator Version1, use version 1.037P (old version).
Language
English
Overview
- The motion control setting is software that is used with GX Works3 to configure settings and perform monitoring for Motion modules.
- Version 1.005F or later does not support the motion system software version 04 or earlier.
Use version 1.001B (old version) when communicating with RD78G4/RD78G8/RD78G16/RD78G32/RD78G64 which has a motion software version of 04 or earlier.
Target model name
SW1DNN-MUCNF-E
Target engineering tool
GX Works3
CW Configurator Version1
Software
Name | Version |
Size
(Bytes)
| Update date | Downloads |
Motion control setting (English version) Motion system software version 05 and later (supported by RD78G4/RD78G8/RD78G16/RD78G32/RD78G64/RD78GHV/RD78GHW) | 1.055H | 234,907,369 | 2024/07/04 | sw1dnn-mucnf-e_055h.zip |
Motion control setting (English version) For CW Configurator Version1 | 1.037P | 235,206,114 | 2022/07/28 | sw1dnn-mucnf-e_037p.zip |
Motion control setting (English version) Motion system software version 04 or earlier (supported by RD78G4/RD78G8/RD78G16/RD78G32/RD78G64) | 1.001B | 106,423,614 | 2019/09/06 | sw1dnn-mucnf-e_001b.zip |
Supported OS
Major new functions added in motion control setting Ver. 1.055H (July, 2024)
No. |
Contents |
2 |
Object data settings can now be changed in the Axis Parameter Setting screen according to the drive unit used. |
4 |
The following functions are supported by operation profile data (multiple axes positioning data):
- Setting skip signals
- Adding PROFILE_POSITIONING_DATA_EXTENDED structures |
Major improvement history from motion control setting Ver. 1.050C to 1.055H (July, 2024)
No. |
Contents |
8 |
Solved a problem whereby when setting signals to be used as external signals for control (for example, the upper limit signal of a real drive axis), users could not specify a string exceeding 63 characters. |
23 |
Solved a problem whereby performing Convert/Rebuild All after certain operations (adding a POU containing an FB after doing a search/replacement) would result in an "Invalid device or invalid constant is used" error. |
Notes regarding improvement history
- The improvement history describes the main contents.
- The actual cases may differ from the description depending on the customer's condition of use, etc.
Precautions for file use
- Install the file on a personal computer where SW1DND-GXW3-E has been installed.
- Please read the word "DVD-ROM" in the message on the installation screen as "the downloaded folder".
Procedure for extracting a compressed file
Download the file to any folder.
Decompress the downloaded file, which will create a sw1dnn-mucnf-e_xxxx folder (xxxx varies by the version).
Extraction method 1) Using an OS that has a Zip file extraction function
- Right-click the downloaded file.
- Select "Extract all"
If "Extract all" is not displayed, execute extraction method 2).
- Specify the destination and click "Extract".
Extraction method 2) Using an OS that does not have a Zip file extraction function
- Obtain a ZIP extraction tool if you do not have one.
- Use the tool to extract the files. Extract the files with a specified directory.
* Please use the extraction tool at your own risk.
Installation method
- Execute sw1dnn-mucnf-e_xxxx.exe in the sw1dnn-mucnf-e_xxxx folder (xxxx varies by the version).
- Install the motion control setting by following the messages on the installer.