Firmware - Motion module - MELSEC iQ-R Motion module motion system software
English, Japanese
Motion system software for MELSEC iQ-R series Motion modules
RD78G4, RD78G8, RD78G16, RD78G32, RD78G64, RD78GHV, RD78GHW
Name | Version |
Size
(Bytes) | Update date | Downloads | Remarks |
---|---|---|---|---|---|
Motion system software 34 | 34 | 13,620,584 | 2024/07/04 | sw12dnn-rmtufw_34.zip | Boot version 16 Latest |
Motion system software 33 | 33 | 13,560,131 | 2023/12/14 | sw12dnn-rmtufw_33.zip | Boot version 15 |
Motion system software 32 | 32 | 13,559,588 | 2023/12/14 | sw12dnn-rmtufw_32.zip | Boot version 15 |
Motion system software 31 | 31 | 13,424,835 | 2023/10/04 | sw12dnn-rmtufw_31.zip | Boot version 14 |
Motion system software 30 | 30 | 13,424,838 | 2023/05/15 | sw12dnn-rmtufw_30.zip | Boot version 14 |
Motion system software 28 | 28 | 13,411,401 | 2023/02/28 | sw12dnn-rmtufw_28.zip | Boot version 13 |
Motion system software 26 | 26 | 13,335,764 | 2022/12/02 | sw12dnn-rmtufw_26.zip | Boot version 12 |
Motion system software 24 | 24 | 13,537,276 | 2022/06/30 | sw12dnn-rmtufw_24.zip | Boot version 11 |
Motion system software 22 | 22 | 13,121,883 | 2022/03/30 | sw12dnn-rmtufw_22.zip | Boot version 10 |
Motion system software 21 | 21 | 13,121,989 | 2022/02/04 | sw12dnn-rmtufw_21.zip | Boot version 09 |
Motion system software 20 | 20 | 13,121,746 | 2021/10/26 | sw12dnn-rmtufw_20.zip | Boot version 09 |
Motion system software 18 | 18 | 13,050,001 | 2021/06/24 | sw12dnn-rmtufw_18.zip | Boot version 08 |
Motion system software 17 | 17 | 13,049,031 | 2021/05/31 | sw12dnn-rmtufw_17.zip | Boot version 08 |
Motion system software 16 | 16 | 13,023,754 | 2021/05/07 | sw12dnn-rmtufw_16.zip | Boot version 07 |
Motion system software 14 | 14 | 11,119,107 | 2021/01/20 | sw12dnn-rmtufw_14.zip | Boot version 06 |
Motion system software 13 | 13 | 11,116,188 | 2020/11/30 | sw12dnn-rmtufw_13.zip | Boot version 05 |
Motion system software 12 | 12 | 11,115,478 | 2020/11/30 | sw12dnn-rmtufw_12.zip | Boot version 05 |
Motion system software 10 | 10 | 11,091,685 | 2020/07/30 | sw12dnn-rmtufw_10.zip | Boot version 05 |
Motion system software 09 | 09 | 11,041,950 | 2020/05/28 | sw12dnn-rmtufw_09.zip | Boot version 04 |
Motion system software 08 | 08 | 11,042,724 | 2020/05/28 | sw12dnn-rmtufw_08.zip | Boot version 04 |
Motion system software 07 | 07 | 10,826,733 | 2020/03/26 | sw12dnn-rmtufw_07a.zip | Boot version 03 |
Motion system software 05 | 05 | 10,804,697 | 2019/12/20 | sw12dnn-rmtufw_05.zip | Boot version 03 |
Motion system software 04 | 04 | 7,570,307 | 2019/10/02 | sw12dnn-rmtufw_04.zip | Boot version 02 |
Click here for the installation method.
Manual | IB-0300411ENG-J | MELSEC iQ-R Motion Module User's Manual (Application) | [ English ] |
---|
○:Applicable,-:Not applicable
No. | Contents | PLCopen® motion control FB mode |
Simple Motion mode |
---|---|---|---|
1 | In MCv_MovePositioningData (Multiple Axes Positioning Data Operation) now supported the following functions. - skip functions - step functions - read/write condition and skip signal in operation profile (positioning data format) |
○ | - |
2 | Support for connection to drive units other than MELSERVO. | ○ | - |
3 | Speed bias function supported. | ○ | - |
4 | In advanced synchronous control, support for synchronization encoder axes via link devices has been added. | - | ○ |
5 | In the mark detection function, support for input signals from link devices has been added. | - | ○ |
○:Applicable,-:Not applicable
No. | Contents | PLCopen® motion control FB mode |
Simple Motion mode |
---|---|---|---|
1 | Improvements have been made to enable "Connected/Disconnected Module Detection" to be performed when the motion unit is not data-linked. | ○ | ○ |
When installing the motion system software version 08 or later, the basic system software and the boot software can be installed simultaneously by batch installation.
How to batch install the boot software and the basic system software
The boot software and basic system software cannot be installed simultaneously by version 07 or earlier.
Install the basic system software/add-ons after installing the boot software.
For details of the installation method, refer to "MELSEC iQ-R Motion Module User's Manual (Application)".
Precautions
The built-in memory must be cleared after updating the software from version 04 or earlier to version 05 or later.
The built-in memory clear deletes the following data including the absolute position data. Back up and restore data as required before and after the built-in memory clear.
The built-in memory clear and data backup/restoration are executed on the motion control setting.
Procedure for built-in memory clear and data backup/restoration (If data backup/restoration is not necessary, skip step 2, 3, 4, 8, and 9)