e-Manual is the electronic books that enable Mitsubishi Electric FA product users to quickly obtain necessary information such as product ranges and usage.
Excellent search functions and the linkage with engineering software facilitates the start-up and maintenance of FA products. User maintenance manuals can be easily converted into e-Manual files and linked to Mitsubishi Electric FA product manuals, enabling quick troubleshooting.
When an error or trouble occurs in an FA product at a production line, you can check its causes and corrective actions described in troubleshooting in applicable manuals on a computer.
Cross search across all downloaded manuals is available.Also, refine search with key words such as error codes or programming commands enables quick search.
Required information can be cross-searched in multiple manuals. Cross search across all downloaded manuals is available. Also, refine search with key words such as error codes or programming commands enables quick search.
Product name
Manual number
Illustration
Keyword
Fuzzy term
Error code
Description of a special relay
Description of a special register
Description of a command
Information on a note
Page ID
By using the bookmarking function, frequently accessed maintenance or troubleshooting information pages can be immediately found when required at manufacturing sites. Registered bookmarks will be copied onto updated manuals.
User documents can be freely customized by adding notes about know-how and information required for system start-up and maintenance. Added notes will be copied onto updated manuals.
By storing e-Manual data (manuals, notes, bookmarks) in a database on the network, team members can share and view the latest documents with notes on their computers. Downloading the same manuals repeatedly will be no longer necessary and data capacity on each computer can be reduced.
By exporting e-Manual data (manuals, notes, bookmarks) saved in e-Manual Viewer, users can transfer the same data to other computers. For example, a user can export e-Manual data saved in e-Manual Viewer on their computer at the office to a notebook computer used for manufacturing sites or business trips. Also, they can use it as backup data when the computer is restored.
Sample programs provided in e-Manual can be copied with one click. They are pasted to a project on engineering software to ready for running. Program input can be quicker and mistakes can be prevented. This helps users streamline the start-up of the FA products.
The distribution and update service of e-Manual Viewer application for the tablet (Android™ and iOS) version on Google Play and App Store ended at the end of March 2024.
The application you are currently using will be continuously available even after each store discontinues the distribution.
If you want to use e-Manual Viewer on tablets, please use the tablets whose operating system is Windows®.
Google Play is the trademark of Google LLC.
Operating system version | Operating confirmed device |
---|---|
Windows® 10 or later | Windows® 11, Windows® 10 |