Factory Automation

MELSERVO-JET Series Servo Amplifier Features

MELSERVO-JET Series Servo Amplifiers

MR-JET-G
  • CC-LinkIE TSN
  • MR-JET-G *1

Supports Ethernet-based CC-Link IE TSN, featuring high-speed, large-capacity communication (1 Gbps).
Communication cycle of ≥ 125 μs and speed frequency response of 2.5 kHz enable advanced motion control.

  • *1.MR-JET-G also supports CC-Link IE Field Network Basic.
MR-JET-G-N1
  • EtherCAT
  • MR-JET-G-N1

MR-JET-G-N1 servo amplifiers support EtherCAT®.
(100 Mbps)

Compact Servo Amplifiers with Simple Wiring

Simple, Efficient Wiring

The servo amplifier offers simple wiring by having connectors on the top and bottom surfaces, and allows all cables and wires to be routed through wiring ducts. LEDs and switches are located on the front surface of the servo amplifiers for easy operation.

Simple, Efficient Wiring

Tuning Functions

Use the tuning methods that are optimal for your machines.

Use the tuning methods that are optimal for your machines.

Quick Tuning

This function automatically performs easy-to-use auto tuning that controls vibration and overshoot just by turning on the servo-on command. Before normal operation, the servo amplifier sets control gain and machine resonance suppression filters in 0.3 seconds by inputting torque to the servo motor automatically. After completing the setting, the servo amplifier starts operation normally.

Quick Tuning

One-Touch Tuning

This function automatically completes servo gain adjustment according to the mechanical characteristics and reduces the settling time just by turning on the one-touch tuning. The servo gain adjustment includes the machine resonance suppression filter, advanced vibration suppression control II, and the robust filter. Controlling overshoot and vibration is improved, maximizing your machine performance.

One-Touch Tuning

Advanced Vibration Suppression Control II

This function suppresses two types of low frequency vibrations, owing to vibration suppression algorithm which supports three-inertia system. This function is effective in suppressing residual vibration with relatively low frequency of approximately 100 Hz or less generated at the end of an arm and in a machine, enabling a shorter settling time. Adjustment is easily performed on MR Configurator2.

Advanced Vibration Suppression Control II

Command Notch Filter

The frequency can be set close to the machine vibration frequency because the command notch filter has an applicable frequency range between approximately 1 Hz and 2000 Hz.

Machine Resonance Suppression Filter

The expanded applicable frequency range is between 10 Hz and 8000 Hz. Five filters are simultaneously applicable, improving vibration suppression performance of a machine. The machine resonance frequency is detected by the machine analyzer function in MR Configurator2.

Preventive Maintenance

Machine Diagnosis Function

This function detects changes in mechanical parts (ball screw, guide, bearing, belt, etc.) by analyzing changes in machine friction, load moment of inertia, unbalanced torque, and vibration components from the data inside a servo amplifier, supporting timely maintenance of these parts.

Machine Diagnosis Function

Servo Amplifier Life Diagnosis

This function displays the cumulative energization time and the number of inrush relay on/off times. The data can be used to check the service life of the parts as a rough guide.

  • Cumulative energization time (Smoothing condenser/cooling fan life span)
  • The number of inrush relay on/off times (Inrush relay life)
Servo Amplifier Life Diagnosis

Corrective Maintenance

Drive Recorder

This function continuously monitors the servo status and records the status transition such as a trigger condition before and after an alarm for a fixed period of time. Reading the servo data on MR Configurator2 helps you analyze the cause of the alarm. In addition to the monitor values and the waveform of the past 16-time alarms in the alarm history, the system configuration and the servo parameters are displayed. Alarm occurrence time is also displayed when the servo amplifier and the controller are normally in communication on CC-Link IE TSN.
The data can be outputted to a GX LogViewer format file.

Servo Amplifier Drive Recorder

Connection/Communication Diagnosis

Disconnection Detection

The servo amplifiers detect an open phase condition on the output side. The alarm can be distinguished from other alarms such as the overload alarm, reducing the time required to restore the system.

Disconnection Detection

Encoder Communication Diagnosis

The encoder communication diagnosis checks the encoder communication circuit in the servo amplifier. This function is useful for classifying the cause of errors (such as disconnected encoder cables) when the encoder communication alarm occurs.

Encoder Communication Diagnosis

Path Control

Super Trace Control

This function reduces a position deviation to nearly zero not only during constant-velocity operation, but also during constant acceleration/deceleration.
The path accuracy will be improved in high-rigidity machines.

Super Trace Control

Lost Motion Compensation

This function suppresses quadrant protrusion caused by friction and torsion generated when the servo motor rotates in a reverse direction.
Therefore, the accuracy of circular path will be improved in path control used in XY table, etc.

Lost Motion Compensation

Path Tracking Model Adaptive Control

This function reduces path errors which occur when the servo motor reciprocates.
Normally, when positioning control is executed, the model adaptive control adjusts the control to shorten a settling time. Instead, this function reduces overshooting to improve path accuracy, which is suitable for machines that require high-accuracy path control such as processing machines.

Path Tracking Model Adaptive Control

Supporting Flexible Driving System

Fully Closed Loop Control

Enhanced
functions

Supporting a fully closed loop control system as standard *1, the servo amplifiers enable further precise positioning.

  • *1.The servo amplifiers are compatible only with two-wire type serial encoders.
    Use the servo amplifier manufactured in July 2022 or later.
    Note that, depending on the stock status, the servo amplifiers with both the former and the new specifications may be distributed in the market around the same time. Contact your local sales office when the fully closed loop control is needed.
Fully Closed Loop Control

Touch Probe Function

Enhanced
functions

When a touch probe (sensor) that detects the position of workpieces is connected to a servo amplifier, the touch probe function latches (stores) the position detected by the touch probe. The controller reads and uses the latched value for position correction. The latch accuracy of this function is 1 μs.*1

  • *1.Use the servo amplifier manufactured in July 2022 or later.
    Note that, depending on the stock status, the servo amplifiers with both the former and the new specifications may be distributed in the market around the same time. Contact your local sales office when the touch probe function is needed.
Touch Probe Function

Positioning by Using a CC-Link IE TSN-Compatible RJ71GN11-T2

An RJ71GN11-T2 master/local module that supports CANopen can control the servo amplifiers.*1
The servo amplifiers support both the profile mode (position/velocity/torque) and the positioning mode (point table). *2
With these operation modes, a positioning system can be simply configured without a Positioning module. In the profile position mode, for example, the target positions and speeds can be set from the master station. The servo amplifier generates commands to the target positions with a start signal and starts positioning operations.

  • *1.RD78G/FX5-SSC-G Motion modules also support CANopen.
  • *2.For the modes supported by the master station, refer to the master station specifications.
Profile position mode continuous operation/Profile position mode continuous operation (point table)

Command Interface

CC-Link IE TSN JET-G

The servo amplifiers receive commands (position/velocity/torque) from a CC-Link TSN-compatible controller at regular intervals through synchronous communication and drive the servo motors.
When combined with a Motion module or Motion Control Software, the servo amplifiers perform exact synchronous operation of axes and machines through high-speed, high-precision time synchronization.
The servo amplifiers support CiA 402 drive profile and enable the profile mode (position/velocity/torque) and the positioning mode (point table). When combined with the controllers supporting the profile mode, the servo amplifiers generate a positioning command to a target position, reducing loads of the controllers.

CC-Link IE TSN

CC-Link IE Field Network Basic JET-G

CC-Link IE Field Network Basic-compatible master stations such as an FX5U CPU module can control MR-JET-G servo amplifiers. The servo amplifier can be operated as a CANopen device via a link device.
The profile mode (position/velocity/torque) and the positioning mode (point table) are supported.
MR-JET-G servo amplifiers can be connected to existing systems using MR-JE-C.
In addition, MR-JET-G supports the line topology. *1

  • *1.When a device which does not support the line topology is used, the line/star mixed topology is applicable.
CC-Link IE Field Network Basic

EtherCAT® JET-G-N1

Configure an EtherCAT® system with the high-performance MR-JET series servo amplifiers.
MR-JET-G-N1 servo amplifiers support EtherCAT®.

Communication specification CANopen over EtherCAT® (CoE)
Drive profile CiA 402
Communication cycle 125 μs, 250 μs, 500 μs,
1 ms, 2 ms, 4 ms, 8 ms
Control mode Cyclic synchronous position mode (csp)
Cyclic synchronous velocity mode (csv)
Cyclic synchronous torque mode (cst)
Profile position mode (pp)
Profile velocity mode (pv)
Profile torque mode (tq)
Homing mode (hm)
EtherCAT

Related Link