News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
Mitsubishi Electric to Expand Lineup of J1-Series High-power Semiconductor Modules
New modules in compact packages for electric and hybrid vehicles
![](/news/images/common/1pix.gif)
Samples will be exhibited at Power Conversion Intelligent Motion (PCIM) Europe 2015 in Nuremberg, Germany from May 19 to 21 and the Automotive Engineering Exposition in Yokohama, Japan from May 20 to 22, and PCIM Asia 2015 in China from June 24 to 26.
![](/news/images/common/1pix.gif)
Power modules for automobiles must deliver higher reliability than industrial-use modules due to the extremely high standards for vehicle safety. Mitsubishi Electric pioneered the mass production of power modules for hybrid vehicles in 1997, and since then the demand for these modules has grown in parallel with the expanding global market for electric and hybrid vehicles. The new high-power J1-Series modules feature compact packages with small footprints, low power loss and high reliability for use in the inverters of electric and hybrid vehicles.
Series | Model | Specifications | Shipment |
J1-Series | CT1000CJ1B060 | 650V/1000A (6-in-1 package) |
Oct. 2015 |
CT600CJ1B120 | 1200V/600A (6-in-1 package) |
Dec. 2015 |
1) | Extra-compact package for automotive inverters
|
||||
2) | Low power loss and high reliability for automotive power train
|
||||
3) | Suppresses surge voltage through internal inductance reduction
|
J1-Series power modules are compliant with the Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment (RoHS) directive 2011/65/EU.
![](/news/images/common/1pix.gif)