- Research & Development
- Energy Systems
- Factory Automation Systems
FOR IMMEDIATE RELEASE No. 3290
TOKYO, July 8, 2019 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed what is believed to be the world's first diagnostic technology based on the company's proprietary Maisart®* artificial intelligence (AI) technology that uses machine learning to analyze sensor data and then generate a model of a production machine's transition between various operational states, thereby enabling the technology to detect machine abnormalities rapidly and accurately for improved productivity in factories and plants.
- * Mitsubishi Electric's AI creates the State-of-the- ART in technology
Conventional and new abnormality-detection technologies
Key Features
- 1)Uses AI for accurate detection of machine abnormalities based on model of operational transitions
- Unlike conventional diagnostic technology, which uses the same conditions for abnormality detection regardless of a machine's current operational state, the new AI technology analyzes sensor data to automatically generate a model of the machine's transition between various operational states, and then uses the model to set optimal conditions for detecting abnormalities during each operation.
- Signs of machinery failure can be detected accurately prior to actual breakdowns, helping to reduce the labor associated with performing maintenance and dealing with downtime in factories and plants.
- 2)AI simplifies introduction of abnormality-detection systems
- The new AI technology eliminates complicated manual settings to simplify the introduction of abnormality-detection systems.
Inquiry
Media contact
Customer Inquiries
Related articles
- Research & Development
-
Sep 19, 2024
-
Jun 13, 2024
-
May 20, 2024
- Energy Systems
-
Aug 28, 2024
-
Jul 17, 2024
-
Jun 28, 2024
- Factory Automation Systems
-
Jun 13, 2024
-
May 29, 2024
-
May 27, 2024