- Research & Development
- Semiconductors & Devices
FOR IMMEDIATE RELEASE No. 3344
TOKYO, March 25, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed a new technology to integrate power devices, passives, sensors and other embedded components in the same substrate, which the company deployed in a 100kW (continuous) bidirectional DC-DC converter to achieve what is believed to be the world's most power-dense* power converter, rated at 136kW/L, or eight times more power dense than conventional converters. The new technology is expected to contribute to the downsizing of power electronics equipment.
- *According to Mitsubishi Electric research as of March 25, 2020
![Demonstrator of new 136kW/L (24×18×1.7cm) high-power-density power c](/mobile0c9a66/sites/news/2020/images/0325.jpg)
Key Features
Mitsubishi Electric's new integration technology enables the parasitic inductance of the switching current loop to be reduced to less than 1/10th that of conventional converters. The resulting clean switching allows high-speed commutation for high-operating frequencies in silicon-carbide (SiC) metal-oxide semiconductor field-effect transistors (MOSFETs). The technology leads to considerably smaller passive components, such as reactors for current smoothing, and capacitors, which take up much space in DC-DC converters.
Inquiry
Media contact
Customer Inquiries
Related articles
- Research & Development
-
Jun 13, 2024
-
May 20, 2024
-
Mar 26, 2024
- Semiconductors & Devices
-
Jun 14, 2024
-
Jun 10, 2024
-
Jun 06, 2024