- Research & Development
FOR IMMEDIATE RELEASE No. 3494
TOKYO, February 28, 2022 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it has developed a teaching-less robot system technology to enable robots to perform tasks, such as sorting and arrangement as fast as humans without having to be taught by specialists. The system incorporates Mitsubishi Electric's Maisart®1 AI technologies including high-precision speech recognition, which allows operators to issue voice instructions to initiate work tasks and then fine-tune robot movements as required. The technology is expected to be applied in facilities such as food-processing factories where items change frequently, which has made it difficult until now to introduce robots. Mitsubishi Electric aims to commercialize the technology in or after 2023 following further performance enhancements and extensive verifications.
- 1 Mitsubishi Electric's AI creates the State-of-the- ART in technology
![](/mobile0c9a66/sites/news/2022/images/0228-1.jpg)
Overview
Processes | Results | |
Conventional Technology | Environmental information: Prepared by experts using CAD, etc. Program entry: Manual. Adjustments/modifications: Confirmed using simulator and/or trial and error. |
|
New Self-programming Technology | Environmental information: Prepared by system using sensors Program entry: Via tablet or voice. Adjustments/modifications: Self-programmed commands optimize motion trajectory and timing |
|
![](/sites/news/2022/images/0228-2.jpg)
Fig. 1 Example of increased efficiency achieved with new system
Inquiry
Media contact
Customer Inquiries
Related articles
- Research & Development
-
Jun 13, 2024
-
May 20, 2024
-
Mar 26, 2024